This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF45EVM: HSDC Pro 4.70 version can't select the ADC tab, and select "ADC32RF34_8224" using the drop-down menu in HSDC Pro With Xilinx® KCU105

Part Number: ADC32RF45EVM
Other Parts Discussed in Thread: ADC32RF45

Hi.

I am designed ADC32RF45EVM  board and KCU105EVM Board.

ADC32RF45EVM With KCU105 Board Setup Example in "HSDC Pro With Xilinx® KCU105 User guide (SLAU711–March 2017)"

Set up the hardware as follows:

1~9 is ok.

but, "10. Open HSDC Pro, select the ADC tab, and select "ADC32RF34_8224" using the drop-down menu" is not supported in HSDC Pro 4.70.

but, i can't see "ADC32RF45_8224" in drop-down menu.

i want to this example completed.

what is problem?

Help me please.

  • Hi Kim,

    It looks like this INI file was not included in the release. Someone will look into this and get back with you soon.

    Ken.
  • im,

    It looks like 2 INI files for ADC32RF45 did not make it into the HSDC Pro release.  I have attached the missing INI - can you please put this into the ADC Files folder and see if it works ok?

    C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro\KCU105 Details\ADC files

    Ken.

    ADC32RF45_8224.zip

  • hi ken C

    thank you for your help.

    i will try .ini file and reply result as soon.

    thank you very much. 

  • hi ken.

    i try ini file.

    but, error message bellow.

    "configure ADC
    CMD_EXEC_ERROR
    error when control command fails"

    what is the problem? do you know?

    please, help me...

    Regards,

    kim
  • Kim,

    Did you load the FPGA using Vivado before running HSDC Pro? What is the status of the LED's on the KCU105? What configuration file did you load the ADC EVM with? Can you send a screen shot of HSDC Pro GUI?

    Regards,

    Jim

  • hi Jim,

    thank you for your reply.

    1.  i'm download “C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro\KCU105 Details\Firmware\KCU105_TI_DHCP.bit".

    2.  KCU105 Board Status and User LEDs are all green. (DS2-init, DS3-OR'D POWER GOOD, done....)

    3. adc32rf45evm configuration file? i'm bypass mode setting in GUI.

    "HSDC Pro With Xilinx® KCU105" file version SLAU711–March 2017. see it

    Regards,

    Kim

  • Kim,

    1. We need to make sure if the FMC Voltage is set as per page 8 in KCU105 User's Guide

    2. DCLK Divider in the ADC should be set as required as per point 6 and 7 in page 19 in KCU105 User's Guide

    Regards,

    Jim

  • hi Jim,

    i'm Set up the hardware as follows completed bellow.

    6.2 Programing the FPGA
    6.3 Adjusting FPGA FMC Settings
    6.4 IP Address and Connecting to HSDC Pro
    7.3 ADC32RF45EVM With KCU105 Board Setup Example

    7.2.10 Open HSDC Pro, select the ADC tab, and select "ADC32RF34_8224" using the drop-down menu.
    as i know, "ADC32RF34_8224" is mistake.

    Regards,

    Kim
  • Kim,

    Is your setup now working? I cannot tell by your latest response.

    Regards,

    Jim 

  • hi ken,

    I am designed ADC32RF45EVM  board and TSW14J56-REV D EVM Board.

    and High Speed Data Converter Pro v4.70 -> v4.00 down-grade.

    i'm example project completed. but, ADC32RF45EVM  board and KCU105 Board are still does not work.

    "ADC32RF45_8224.zip" file is a very usefulled for me.

    thank you very much.

    Regards,

    kim

  • hi Jim,

    I am designed ADC32RF45EVM board and TSW14J56-REV D EVM Board.

    and High Speed Data Converter Pro v4.70 -> v4.00 down-grade.

    i'm example project completed. but, ADC32RF45EVM board and KCU105 Board are still does not work.

    ADC32RF45EVM board setup is same. i think a KCU105 board setup is problem.

    but, i don't know any idea what is problem.

    thank you for your help.

    Regards,

    kim
  • Kim,

    See if these files help.

    Regards,

    Jim

    ADC32RF45_KCU105_files.zip