This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC08B3000: Large voltage range of single-end input

Part Number: ADC08B3000
Other Parts Discussed in Thread: LMH6555, LMH6554

Hi,

My customer is using ADC08B3000.
He wants to input Vin+/- single-end input signal.

The method of inputting single-end signal is showed Figure 46 in datasheet.
But customer condition is that input signal(single-end) range is 0V~4V.

I think that LMH6555 can not receive the input range and AD Converter can not receive the input range. 

Could you let me recommend fully differential amp and circuit at this situation, please?

Best regards,
Shimizu