Hi team,
My customer is using ADS1220 in their O2 detection project. They use it to measure two input signal, one differential pair used to measure O2 sensor input signal; Another sensor is 2-wire RTD.
As we can see from datasheet P55 figure78, the recommended ratiometric measurement circuit need 3 AINx pins. But there is only two AINx pins left, so I wander if we can use (take the circuit on P55 as example) AIN1 to our put the IDAC, and also use AIN0, AIN1 to measure the differential input voltage of RTD. From the input structure on P20 figure38, I think AINx pins can be the IDAC output and voltage input same time, but I’m just not sure. So please give some suggestions to this problem.
Thanks and Best Regards,
Will