This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We have DAC5682Z DAC on FMC interfaced to Virtex 6 FPGA and CDCE72010 for input clock. I have been using it at 250 MSps for generating waveforms without any problem for a few years. But when I tried higher sampling rates I got some bizarre results. I conducted tests at 500 MSps and 1 GSps and here is what I observed:
|
Main Clock(MHz) |
Data Clock(MHz) | Data Waveform*(MHz) | DAC Output(MHz) | Expected DAC output(MHz) |
| 250 | 125 | 125 | 125 | 125 |
| 500 | 250 | 250 | 125 | 250 |
| 500 | 250 | 125 | 62.5 | 125 |
| 1000 | 500 | 500 | 166.667 | 500 |
*data waveform is alternating extremes.
I have turned off interpolation filters and PLL and am setting config 10 for DLL as per table 7.7 in data sheet. I am also sending appropriate sync event after every 125M cycles,
I thing I am missing something very trivial that is resulting in these weird factors of 2 and 3, and would appreciate any help in resolving this.
Thanks in Advance.
Regards,
Arpit.
Hi Neeraj,
Here are some frequency combinations that I tried:
CLK - 1000 MHz DCLK - 500 MHz Data - 500 MHz Output - 166.667 MHz
CLK - 1000 MHz DCLK - 500 MHz Data - 250 MHz Output - 83.333 MHz
CLK - 500 MHz DCLK - 250 MHz Data - 250 MHz Output - 125 MHz
CLK - 500 MHz DCLK - 250 MHz Data - 125 MHz Output - 62.5 MHz
CLK - 250 MHz DCLK - 125 MHz Data - 125 MHz Output - 125 MHz
Regards,
Arpit.