This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3482EVM: Operating DAC3482EVM with TSW1406

Part Number: DAC3482EVM
Other Parts Discussed in Thread: DAC3482, CDCE62005, DAC3484

I'm trying to operate DAC3482 EVM (250 MHz. dual DAC, 16 bit resolution with interpolation).

I connected 6V, operated the software and input some CSV files. I tried a file given to me by TI (50 + 100 MHz. sine waves) and I get only random noise.

I also anoter file that I made - DC on one channel and a sine wave on the other one (see picture below). I still get weird signals. I did FFT of both channels using my oscilloscope - no peaks.

I attach a picture of my board. Could you please tell me what did I do wrong?

  • Hey Aronii, 

    You say your using interpolation but i dont know what your DAC clock is nor do i know your interpolation factor. 

    Try using the configuration file i am attached below to configure the DAC3482EVM. The setting is for 1228.8M Dac clock with 4x int. which means your data rate in HSDC pro should be set to 307.2M.  

    Reference the following user guide to make sure that your jumper settings and FPGA clock frequencies are correct. 

    http://www.ti.com/lit/ug/slau432a/slau432a.pdf

    Yusuf

       x00	   xF28C
       x01	   x0000
       x02	   x8052
       x03	   xA001
       x04	   x4DF1
       x05	   x0000
       x06	   x3400
       x07	   xFFFF
       x08	   x0000
       x09	   x8000
       x0A	   x0000
       x0B	   x0000
       x0C	   x05A6
       x0D	   x05A6
       x0E	   x05A6
       x0F	   x05A6
       x10	   x3000
       x11	   x0000
       x12	   x0000
       x13	   x0000
       x14	   x0000
       x15	   x0640
       x16	   x0000
       x17	   x0640
       x18	   x205F
       x19	   x10F4
       x1A	   x4820
       x1B	   x0800
       x1C	   x0000
       x1D	   x0000
       x1E	   x1111
       x1F	   x8882
       x20	   x2400
       x22	   x1B1B
       x23	   x001F
       x24	   x1000
       x25	   x7A7A
       x26	   xB6B6
       x27	   xEAEA
       x28	   x4545
       x29	   x1A1A
       x2A	   x1616
       x2B	   xAAAA
       x2C	   xC6C6
       x2D	   x0004
       x2E	   x0000
       x2F	   x0000
       x30	   x61A8
       x7F	   x0001
    CDCE62005 Registers
    Freq:19.200000MHz
    Address	Data
    00		80400000
    01		813C0001
    02		81400002
    03		C10C0003
    04		00040004
    05		29F01A55
    06		44AF0006
    07		165294A7
    08		20001808

  • The TXT file that you sent is the default file which comes with the DAC3482 software. Files are identical.

    In the DAC software we do "load regs". We selected your file. Then we did "send all"

    On the TSW1406 software we selected "DAC" tab and then DAC8432. Then we clicked "Load external pattern file" and downloaded the excel CSV file that I attached before.

    (Sine waves.csv). Then we did "SEND". We still don't see anything.

    Did we do anything wrong? The bord is connected directly to the oscilloscope. Is it OK?

  • I forgot to mention that we use the internal CDCE62005 chip - not an external clock. So we changed JP5 to positions 2-3 (shorted) instead of the default. It stil doesn't work.
    We measured the DAC clock at R71, R72 and we get a sine wave of about 125 MHz. riding on DC - not even close to 307 MHz.
    It seems that the setup file for the CDCE62005 is different.
    We don't get any clock at J12 or J15 (we use a 1.5 GHz analog input LECROY scope.
    Please aslo note that eh datasheet that you sent refers to TSW1400 - not to TSW1406.

    Last thing: I clicked by mistake the link to unsubscribe from this thread. Please register me again. I wish to get a notification by E-mail when you answer.
  • Hey Aronii,

    The TSW1406 doesnt seem to be compatible with that device. You will need to use the TSW1400
    to work with the DAC3484EVM.
    Yusuf
  • IT is DAC3482 not DAC3484 EVM.


    You can see that the DAC3482 EVM is listed in TSW1406 web page

    http://www.ti.com/tool/TSW1406EVM

    and also in the datasheet:


    If this board was not compatible, then I could not select it from the list... (in the software)

    I also asked in the forums about operating both boards together before I bought them and no one told me that they don't work together.

    I wonder where did you read it?

    The difference between the boards is the speed. I don't need it for maximum speed. 1 GBps is OK for my application.

  • Arnii, 

    I see your point. We usually use the TSW1400 when interfacing with the DAC3484 so i will have to put in an order for TSW1406 in order to run some experiments on my end and get back to you. I will check back in with you as soon as I receive the board. 

    Yusuf