Other Parts Discussed in Thread: ADS1298R
I am trying to implement Internal Calibration of ADS1298R.
for that i have configured input it as Test Signal and checking the values at different gain settings.
Test signal amplitude =1 × –(VREFP – VREFN) / 2400 V
so we are configuring Vref as 2.4 v so ans is 2 mV.
It is the correct procedure to check Calibration or not?