This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1263EVM-PDK: ADS1263 EVM dsp not ready

Part Number: ADS1263EVM-PDK
Other Parts Discussed in Thread: ADS1263, ADCPRO

Hi,

I'm having the DSP not ready issue. I was using the ADS1263 EVM kit since couples days now and it was properly working.

After changing the supply from +5V to ±5V, the DSP not ready issue appeared. Not sure the supply have any to do with this fault.

I tried to reinstall the ADCPRO with the ADS1263 plugin which reinstall automatically the MMB0 driver. This do not solved the issue.

I tried to reinstall manually the MMB0 driver as stated in other post without any success.

The NI-VISA USB Devices is listed in the device manager.

Any ideas?

Thanks

Olivier Bergeron