Part Number: DAC34SH84EVM
Other Parts Discussed in Thread: CDCE62005, DAC34SH84
Hi,
I had been using DAC34SH84EVM properly without any defection. Recently I am back to test it and I got problem as below:
The DC power in is set 5.35 V, and its current is overlimited 0.14A??? And the voltage was dropping to 3.8V.
Is it the problem with the power supply or the chip? Do you have any idea what's going on here?
THank you.
L.