Other Parts Discussed in Thread: TIPD188, ADS1261
I'm working on a design to read bridge sensor 350Ohm, supplied at 5V, with a full scale of +/-10mV.
I'm planning to use the ADS1262, in similar configuration described in TIPD188, using the AC mode available with chop mode register.
I've not clearly understand the chop mode function.
My application need to have the following configuration:
- 7200SPS, SINC1 --> 2310Hz bandwith
- td(STDR) = 0.494ms
- DELAY[3:0]=278us
In this condition in single convertion mode (DC) I will reach 1/(0.494ms+0.178ms)= 1295SPS, NOT 7200SPS.
In this condition in single convertion mode (AC) I will reach 2/(0.494ms+0.178ms)= 647SPS, NOT 7200SPS.
For my application 647SPS could be enough, but which in the -3dB bandwidth and the ENOB?
What append if I set the continuous conversion with the chop mode enabled? I don't understand who drive the output pin to reverse the power supply of the bridge, as shown in the TIPD188.
In order to reduce the CPU load of the microcontroller, I plan to read the ADS1262 with a timer of 600Hz and I prefer the the ADS1262 will manage by itself the chop mode. Do you think that there is a way to do it?
Regards
Felice