Part Number: ADS1298
Hello! I'm new to the ADS1298/8R EVM Evaluation Software,
I'm trying to make a few test signals, and when I create an input short to either Lead I or Lead II, aVL and aVF do not match with the definition provided by the manual (aVL = Lead I - (1/2)*Lead II, aVF = lead II - (1/2)*Lead I), because when Lead I = 0, aVF = 0; and when Lead II = 0, aVL = 0.
I suppose it has something to do with the configurations of GPIO and OTHER Registers but I am not sure how to proceed.
Any help is greatly appreciated. Thank you very much!