This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
May I use ADS131A04 in the single-ended application instead of differential(with KX220),
Is there any IC which can replace quickfilter QF4A512
Hello Nitin,
Thanks for your post and welcome to the forum!
To achieve single ended measurements with the ADS131A04 you can use a pseudo differential input configuration, short the negative differential input channel to GND, and enable the negative charge pump. This will allow for single ended measurements down to -1.5V with respect to GND.
I'm not familiar with the QF4A512, so I'm not sure about offering a replacement. Typically, using an RC filter on the analog inputs is sufficient for these devices in combination with the integrated digital filter.