Other Parts Discussed in Thread: SN74LVC2G125
Hello,
I use one SPI interface to communicate with 2 AFE5401. Both have an own Chip Select, but Clock, MISO, MOSI are shared.
I can see data written to the chips at correct Voltage Level.
When reading from one device while the other device is not selected (SEN high), it looks like the 2nd device still drives the SDOUT signal.
I have two resistors in the SDOUT lines (same value 330Ohm) and connect both signals on the processor side (TI TDA2P in this case). The Voltage level is not 3.3V but 1.6V which looks to me that the other SDOUT is at Low level and the voltage is divided with the 2 resistors. I removed one resistor to disconnect the 2nd SDOUT and the level is o.k.
I can not find in the data sheet that SDOUT will go to High-Impedance when CS(=SEN) is high.
I can also see that after reading one word the Level of SDOUT stays at high or low level whatever the last bit was.
Best regards,
Michael.