This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
IDAC0 is not working. IDAC0 Muxed to Ain2 but no current is available.
Michael,
The only thing I can think of is that for your connections, you don't have a connection between REF- and ground. If REF- is floating, there's nowhere for the current to sink and nothing will come out of the IDAC. I think this is a difference between the ADS1247EVM and the ADS1248EVM for the REF- connection.
However, just in case this isn't the problem, I did run a quick alternate test to make sure currents come out of the IDACs. I ran a test with a 1kΩ resistor going from AIN0 to ground. Here's a quick picture of the setup.
Using ADCPro and the ADS1248EVM plugin, I set the Power & Ref tab. I turn on the Internal Reference, set the IDAC magnitude to 1000uA and then set the IDAC to the AIN pins (both IDACs)
Then I go to the I/0 Config tab and set IDAC0 to go to AIN0 and IDAC1 to go to AIN4 (I do this to get it out of the way.
After that, I just measure the voltage across the resistor to verify that the current is there, and I get about 1V across it.
Again, if the REF-/ground connection isn't the problem, I would duplicate my test to see if you can route the current in this way. I would note that the data taken from the application shown in the datasheet comes from this EVM.
Joseph Wu