Hello,
in the datasheet of the TLC2543 the following maximum error values are given :
-Linearity Error = +/-1LSB
- Differential Linearity Error = +/-1LSB
- Offset Error = +/-1.5LSB
- Gain Error = +/-1LSB
- Total Unadjested Error = +/-1.75LSB
Those maximum values are given at 25°C or on the operating free-air temperature range of the component ?
If it is given at 25°C, what is the temperature variation of those errors ?
At 25°C, do you have a random distribution of those errors as for example :
the total error follows a gaussian law and 99.7% (3sigma) of the ADC have a total error of +/-1LSB ?
Best regards,
Nicolas Divel