Part Number: PGA970EVM
Other Parts Discussed in Thread: USB2ANY, PGA970
Using the PGA970GUI and the supplied USB2ANY device for communication with the PGA970EVM.
The PGA970 will not produce any waveform on P1 or P2
I have verified the PGA970 has at least some function by verifying voltage levels and data transfer:
7.5-V, 5-V, and 3.3-V regulators all within 10%
The AVDD and DVDD are also within 10%
I connected an oscilloscope to MOSI and MISO using SPI to communicate, load the FRAM and press Verify FRAM, there is data to and from the PGA970 on pins MOSI and MISO.
When I press Verify FRAM and the FRAM Status gets to 100% the NOT MATCHED "LED" never changes.
I followed the settings found in the PGA970EVM manuals for the ADC settings as well as recommended settings found on ti E2E threads related to the PGA970.
The waveform generator will not produce an output.
measuments are taken related to TP23 ground
when I enable VREF Buffer, the voltage on pin P1 will go from 60mv to 1.8 volts DC and on pin P2 will go to 1.08 volts DC.
the Analog Power has no effect on the P1 and P2
the settings, GAIN_CTRL, SEM, DAC_VCM, DIFF_VOCM all have an effect the DC voltage on pins P1 and P2 a small amount
example:
- GAIN_CTRL = 1 P2 = 1.08vdc
- GAIN_CTRL = 1.67 P2 = .840vdc
MICRO_RESET also has no effect on the P1 and P2 outputs
I removed the jumpers J2 and J7 to verify the LVDT primary is not loading the circuit.
I have verified that I can write to the registers of the MCU by dumping FRAM an DEVRAM also reading the Data & Waveform RAM
Nothing I have tried will produce a wave form, only DC on P1 and P2
mesuements taken related to TP45 ground, P1A and P2A are at 9.2 volts DC