LSB( 0- 3bit) of conversion result of IN4 is always 0x03.( Result is 0x8b83 or 0x8bc3 )
INPUT = 1.65V (D.C.) REF = 3V AVdd = 3.1V DVDD = 3V
Manual trigger mode
Channel select is used
Even if IN4 and IN3 are replaced , it will be the same result.
SPI Lne of ADS8332 are monitored by Oscilloscope.
0x8b83 or 0x8bc3 is output certainly.
I think that ohter results are also obtained .( etc 0x8b84,0x8b85...)
Is thie result is right?
Best regards