Hello,
I'm trying to verify the frequency change after writing the 3 (16 bit) NCO registers. I can write them and then check the SIF SYNC box on the gui and the NCO changes frequency. I wrote to registers 0x11E, 0X11F, and 0x120 three values. I thought the autosync should create the SYNC after the last of these three registers are written. Am I missing something with setting a page bit (which by the way I don't see register 9 or 0x0A show up in the register map in the GUI), or have one of the other settings incorrect?
Thanks,
Jonathan