Part Number: ADS4225
Other Parts Discussed in Thread: ADC3224, , LMK61PD0A2, LMK00304, LMK00334, CDCLVP1204, LMK61E2-125M, THS4541
Hi, i would like to ask you whether using an ADC designed for software defined radio in a DSO project is wrong.
Regarding the DC accuracy section i see nothing that makes me having second thoughts. The input is Differential with a FS magnitude of 2Vpp and the input diff resistance is 750Ω @ 200MHz.
I understand that i have to build the front end accordingly with impedance matching etc.
I went through your 12bit ADCs but all of them had a bandwidth many times greater than the sampling speed which if i am not mistaken means that they are targetting SDR.
So, can a SDR ADC be used in a DSO and perform both in DC & AC coupling well?
Any suggestions? Parts?
Regards
Manos Tsachalidis