Other Parts Discussed in Thread: DDC112
Hello,
I would like to use the DDC112/114 with a photodiode that requires 2 to 9V reverse bias. This operating mode is neither mentioned in the component datasheet nor in the EVM manual. The cathode is always grounded and the anode is connected to the IN- amplifier input. Assuming that it's not possible to add a bias to the IN- input, being the IN+ of the amplifier internally tied to GND, the only solution I see is to connect the cathode to a negative potential.
Is this mode suited for the DD112/114, without compromising the conversion performance?
Do you have other recommendation for the correct use of the DD112/114 with a reverse biased photodiode?
thank you and best
Daniele