Other Parts Discussed in Thread: DAC8811, , PCM1770, PCM1772
Hi,
I have been searching for a DAC to convert decoded mp3 file samples into an analog signal to be fed into an amplifier and speaker. I came across this DAC and am wondering if this would be a good fit for this application. I am targeting a sample rate of 44.1 kHz. I will be interfacing with the DAC using an STM32F4 micro controller (which has a plethora of communication peripherals and high internal clock speed).
I am currently using a DAC8811 along with an I/V converter Op-amp, but I would prefer to use a DAC with an I2C (or I2S) interface.