Other Parts Discussed in Thread: ADS7955, REF5025
Hi there,
I selected ADS7955-Q1 for my application due to cost and temperature grade of 125C. For this ADC, my application consists of measure 6 battery cells (ranging from 10.5V to 15V) thru a voltage divider and input it to the ADS7955, that talks via SPI with MCU.
I based my circuitry in the ADS7955 datasheet and 'ADS79xxEVM and ADS79xxEVM-PDK User's Guide' (http://www.ti.com/lit/ug/slau262d/slau262d.pdf)
Questions:
1. My Vcc is 3V3. Vref for ADS could be 2.5V? (I'm using REF5025)
2. The 33R is to keep input impedance bellow 50Ohm recommended in the Datasheet?
3. This is my input circuitry. Is that ok?
Regards,
Ueliton