Other Parts Discussed in Thread: ADS124S08, ADS1248,
I want to use multichannel scan along with diagnostic flags. I am getting signal from a strain gauge and checked the ADC data and flags in 2 modes i.e.
ScanMode2: One or more channels Continuous Scan
ScanMode3: One or more channels Continuous Scan with Burnout Currents
1. In both cases, i could get the flag status changing. Rail Flags set when I disconnect the transducer in both modes. Then what is the significance of ScanMode3 (with burnout curents)?
2. When would SHORT_THLD_ FLAG be set if I have not set SENDIAG_THLDH and SENDIAG_THLDL values? I can see it setting when the input signal voltage is very high but less than VA. e.g. With VREF and VA set at 5V, and gain 128, OFLO flag sets at 39mv and SHORT_THLD_ FLAG sets at 1.3V.
3. When does POR_AFT_LST_RD flag get set and what is its significance? The datasheet says : Power-on-reset after last read = 1 when there was a power-on-reset event because the last time the SENDIAG_FLAGS register was read. But why would the ADC reset after a read?
Regards,
Naman