This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1220: ADS1220 - question regarding common and differential mode filters for analog and reference inputs

Part Number: ADS1220
Hi Bob,
Thank you very much for your help and suggestions regarding troubleshooting my issues with obtaining reliable SPI communications between ADS1220 part and Raspberry Pi 3.
I completely agree with your comments regarding the advantages of using a single PCB with all the circuitry to reduce any inductance or capacitance caused by wires.
It makes sense that the 100uF caps I added act as reservoirs to supply power to the ADS1220 part when the wire inductance may act to choke the currents required
for operation. I will probably transition to a single board design after my initial testing and development phase is complete. The single board design should help reduce or eliminate the
voltage spikes that I have been seeing and perhaps with the single board design I won't need as large of caps on the ADS1220's digital and analog supplies.
Below is an updated schematic showing the common and differential mode filter caps on the analog inputs as well as the voltage reference to the ADS1220.
Can you please tell me if this looks correct. I am not sure if I should also have series 1K resistances on the REFP0 and REFN0 pins.
Thank you again for your help and time.

-Sean