Hi,
Our customer is considering change from M2510 to M0510.
Customer's Existing model : +/-100A FS, 2m ohm shunt --> +/- 200mV( 4/5 FS of M2510 )
So, I think they should use 0.4m ohm shunt for M0510. (100A * 0.4m ohm = 40mV)
It is correct ?
This is a simple question, but they evaluated it using "0.5"m ohm shunt and it didn't seem to work properly.
If we make the input FS of this device the same, can we replace it directly?
(If not consider noise)
Best regards,
Hiroshi
Best regards,
Hiroshi