Hi,
I am looking into the application design of ADS7039-Q1, in very low speed(~10SPS) data acquisition system. Some inquiries about the datasheet:
tCONV and tACQ - Does the 'acquisition time' refer to the internal S/H capacitor being connected to AINP/AINM pins, while 'conversion time' states the ADC engine running and S/H cap disconnected from AINP/AINM?
I am asking this because it is feasible to sample a very high impedance source(~10MOhm) with extended tCONV period, without external buffer. Any ideas and suggestion are welcomed!
Peiheng.