Other Parts Discussed in Thread: TMS320F28075, TIDA-01094
I will be measuring the inductor current in a dual interleaved boost converter and the inductor current of an inverter.
1) In the examples presented in datasheet of the AMC1304, its used to measure currents of a half bride topology or full bridge, will it work when measuring the inductor current of a boost converter?
2) For powering the AMC1304, I will be stepping down 80V to 12V using an isolated power supply (flyback converter) to power the 12V side of the AMC1304 and an isolated high side low side gate diver, this 12V then gets stepped down again using a non-isolated power supply to 3.3V for powering of a TMS320F28075 dsp and the 3.3V side of the AMC1304. In the datasheet of the AMC1304, a floating power supply is used to power its 12V side. Since I'll be using three AMC1304 for current measurement will my method of power supply work correctly, (80V to 12V isolated) (12V to 3.3V non isolated)?