1.What are the MSPS of DAC128S085
2.What's the difference between A and B, other than the number of channels.Is the protocol the same?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.What are the MSPS of DAC128S085
2.What's the difference between A and B, other than the number of channels.Is the protocol the same?
Hi Hank,
1. The SPI update rate can go > 1.5MHz but the settling time will be the limiting factor. With the 6us settling time, the maximum update rate will be limited to 166 kHz.
2. The DAC128S085 doesn't have A and B variants.
Hope that answers your question.
Regards,
Uttam
.What's the difference between DAC128S085 and DAC124S08, other than the number of channels.Is the protocol the same?
Yes, the protocols are the same. The primary difference is the number of channels.
Thanks,
Paul