Other Parts Discussed in Thread: ADS8860, ADS9120
Hi team,
Recently I study the datasheet of ADS8555, I have two questions about this device,
1. Is it possible to operate the ADS8555 inputs as unipolar while keeping the HVSS at AGND and HVDD at 5V? For this device do not have internal LPF, maybe we can use ii in some application required higher BW.
2. If this application is good, what is the relationship between input voltage range and BINARY CODE?
Thanks.