Other Parts Discussed in Thread: ADS7254, ADS7251
Hi team,
My customer want to find the alternative GPN which can P2P replace the ADS7253IRTER as their second choice.
-
The Resolution should be 12 bits or better and sampling rate should be 1000 ksps or better.
-
The interface should be SPI.
-
The input type should be Pseudo-Differential or Differential
Could you please recommend some GPN ?
- By the way, they don’t accept the ADS7254 as their second choice although the ADS7254 meet the requirement I have mentioned. In their system they have configured the CFR.B7 of ADS7253 to 1, and the CFR.B7 of ADS7254 has to be configured as 0 to set the input mode as Differential. For the consideration of Compatibility in the system, so the ADS7254 is not their good choice
Best Regards,
Wesley Huang
Email: wesley-huang@ti.com