Other Parts Discussed in Thread: TSW1400EVM, AFE5832
Hello, I am working on developing and commercializing a novel ultrasonic transducer technology. To validate its performance, I am looking into commercially available solutions to develop an extendable platform for real-time imaging using these transducers. For the receiving component, the AFE5832EVM board looks to be a promising solution. I have a few initial questions so I can understand its use:
1. Of crucial importance is real-time data capture. Using the software interface and the additional TSW1400EVM, is it possible to get data from the transducers in real-time? And is it possible to get raw data before any software post-processing?
2. The specs for the TSW1400EVM data capture board say it only has eight channels. If we want access to all 32 channels of the AFE5832EVM, will this be possible with a single TSW1400EVM board?
3. Our device will be used for in-air applications at lower frequencies than typical medical devices (our current transducers operate at 300kHz). New transducers can be fabricated to operate at another frequency, but will the AFE5832EVM work at 300kHz?
Thanks in advance for the assistance!