Other Parts Discussed in Thread: TSW1400EVM, AFE5832
Hello,
I had some additional questions regarding use of the AFE5832EVM and TSW1400EVM.
Firstly, in regards to the restriction to eight channels, it is listed in the features of the TSW1400EVM - "up to 8 simultaneous channels". Will we be able to receive data from all 32 channels of the AFE5832EVM simultaneously, or are we restricted to only eight at one time? If we are restricted to eight channels, can we sample all 32 in a lossless fashion, and is there a guide for achieving this easily?
Secondly, is there a guide you could provide us with for accessing the data directly from the TSW1400EVM in a streaming fashion? The user's guide is not clear on this, and a fast setup is very desirable for us. We would like to be able to directly process this data using Python or a similar language.
Thanks again!
Braeden