Other Parts Discussed in Thread: ADS8900B
I've been trying to simulate a circuit taking low and higher level photodiode currents and digitizing them with the ADS8920B. Attached is the schematic I am using. It works fine when the ADC is not in the circuit, then it has convergence problems at the 3mA input when the ADC is inserted back into the simulation. Any idea why I can't get a good simulation with the ADC inline with the input at 3mA?