Part Number: ADS1263EVM-PDK
Other Parts Discussed in Thread: ADS1263
Dear All,
In my group, we are trying to sample an accelerometer signal comes from ADXL354 sensor. The sensor application circuit is shown here 
As shown in the user guide (P22)
, The V1P8ANA pin (no 10 in the application circuit) should be used as a reference voltage in the ADC (I connected it to AIN0 as a REFP). And I connected VSS to AIN1 as a REFN.
Then, I connected the ZOUT signal (single ended signal) to AIN7. I am using a wall adapter to excite the ADC (5V and ground). When I try to sample the signal, I got the all 4 errors (marked with red) appears. When I made the AINN1 to be AINCOM. I got only three errors as shown in the attached photo.
When I press ANICOM, all of them disappears and I got some signal but I am not sure if it is correct what I connected so far because the amplitude of the measured voltage is important to determine the amount of gravity it experiences.