This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: ESD Protection and Absolute Maximum Rating

Part Number: ADS1299


Hello,
we are designing ESD protection for a device, and we wanted to know if the maximum voltage that the IC can withstand in an ESD case on the analog inputs is really Absolute Maximum Ratings, or something else, since it is a voltage pulse.
Additional information: AVDD is 2.5V.
Thanks.