Part Number: ADS7844
Hi,
In the datasheet for the ADS7844, the absolute maximum input voltage rating for the analog inputs is given as -0.3 V to VCC + 0.3 V. However, in the specification table, an "absolute input range" for the negative inputs (when operated in differential mode) is given as -0.2 V to 1.25 V. I believe that "absolute" has been used in this context in order to differentiate from the differential input range rating, and that this should not be interpreted as an absolute maximum rating. (E.g. if a negative input is driven to, say, 1.5 V, the conversion will not be accurate, but no damage will occur.) Is this correct?
Further, the datasheet does not provide default values for the control byte bits (Table III), so it is unclear whether the converter will start up in single ended or differential mode. What is the default value of this register?
Thanks
Shane