Hi Team,
When selection of AMC1035, I have a few questions want to consult.
1) 2.5V reference is generated internally, so whether the resolution of ad is 2.5/2 ^ 16, and whether the output reference REFOUT pin can be used? How to use MCE pin?
2) For analog input (ainp-ainn), the input voltage range is - 1 ~ 1V. If the AC signal is detected, does the positive and negative analog input not need to superimpose the bias voltage, or the positive and negative analog quantity can be directly input. Is there an internal offsets?
Best regards