This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7551-Q1: Temperature Range

Part Number: DAC7551-Q1

DAC Experts,

I'm interested in using the DAC7551-Q1 in an automotive application.  The package size and daisy chaining are attractive for my application, but the temperature range is not.  From an outsiders perspective it looks like there is a very good chance this is the same die as the 6551 with a different bond out.  The 6551 is rated for 125C operation but the 7551 is only rated for 105C, but at the same time the 7551 has a max recommended junction temperature of 150C.  What is the story on the temperature range of this part?  Is this a limitation due to the package?

Thanks,

Trey