Part Number: AMC7834EVM
I seem to be having an issue with the SENSE1 input on the EVM board. I have an input set up that will generate a 0-200mV signal, but the reading I'm getting on SENSE1 continuously bounces between 0 and a high value. If I connect the same circuit to another SENSE input it shows the correct value. Is the SENSE1 input bad or is there something else I'm missing?
I'm including a screen shot of the evaluation interface that shows the same input connected to CS4, the blue line, then moved and connected to CS1, the light green line. As you can see, the value seems to be fine on CS4, but when moved to CS1 it just jumps up and down.