Part Number: AFE0064
Other Parts Discussed in Thread: THS10064, ADS8363, AFE2256
Hi, Team
do you have any guideline or recommendation for selecting ADC for AFE0064? I have some trouble understanding the relationship between the data transfer rate in AFE0064 and the data sampling rate in the following ADC. Is it ok to make the data transfer rate equal to the data sampling rate? For example, I connect the outputs of AFE0064 to an ADC, THS10064. In AFE0064, I set it in sequential mode, and I use a 6 MHz clock signal. The data transfer rate will be 3 MHz. Do you think the outputs from AFE0064 can be sampled by THS10064? Which conversion mode should I use in THS10064 (single conversion mode or continuous conversion mode)?
The reason I choose THS10064 in the previous example is that this is the ADC with 2 differential inputs, multiplexed configuration, and highest sampling rate. If I want to operate AFE0064 at the maximum data transfer rate (7.5 MHz), do you have any suggestions how to convert the analog output signal to digital signal?
Thank you!