Hi Team,
Can you please advise with the request:
"
I am using ADS7953 in a project. There are 6 in a card. And they are all on the same SPI line but with different CS signals. I have to read 16 channels of all integrated circuits consecutively.
All ADS7953 ICs are configured as follows. But the first one works, the others don't. If I configure each one at a time and then read 16 channels, it's okay.
Do you have any suggestions on this subject?
ads7953_Write_Data (port_ADC_SPI_CS1, 0x8000); // Auto-1 Mode - Frame 1
ads7953_Write_Data (port_ADC_SPI_CS1, 0xffff); // Auto-1 Mode - Frame 2
ads7953_Write_Data (port_ADC_SPI_CS1, 0x2c00); // Auto-1 Mode - Programming - Reset Channel Counter
ads7953_Write_Data (port_ADC_SPI_CS1, 0x2800); // Auto-1 Mode - Programming - Incremental channel counter
ads7953_Write_Data (port_ADC_SPI_CS1, 0x2800); // Auto-1 Mode - Programming - Incremental channel counter
"
Thanks in advance
Best Regards
Furkan Sefiloglu