This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
(target C6678, CCS 5.5)
I'm creating a personnalised Perspective based on CCS Debug.
However in the Tools menu : Hardware trace and System Analyser are missing.
In CCS Debug they are present.
I think it's a bug.
You can reproduce it easily :
On a new workspace, open the CCS debug perspective. Right click "save as" MyDebug.
In CCS debug : tools -> Hardware trace and System Analyser are available
In MyDebug : tools -> Hardware trace and System Analyser are missing
Regards,
Clement
Hello Clement,
I see this. It's strange. When you first create the new perspective and then check the menus... it is there. But once you switch perspectives or try to customize the perspective, it disappears. And i can't seem to bring it back via the "Customize perspective" dialog.
let me look into this further...
ki
It seems to be a bug. This should work.
I filed a bug. The tracking ID is: SDSCM00048700
Thanks
ki
"i can't seem to bring it back via the "Customize perspective" dialog."
Neither do I.
This bug is also present on CCS v6 bêta 1.
Clement
By the way : what is more annoying is the "float" conversion missing in the memory browser (affects both CCS 5.5 and 6 bêta1). Do you know if someone is working on it ? I know it is in your bug database.
Clement FR said:Do you know if someone is working on it ? I know it is in your bug database.
Do you know what the tracking ID is?
Clement FR said:The tracking ID is : SDSCM00047876
Looks like it is scheduled for CCSv6 final release