Tool/software: Code Composer Studio
CCS version 7.4.0.00015
I tried both the Web based install on a Win 7.0 64bit machine (new Dell Precision Laptop bought last fall) and the "stand-alone" install and both attempts ended in failure. BTW, the second one successfully sent the install log to the TI support site in the sky to show where the install failed but I have not received any notification of its receipt or contact to help. I thought that the stand-alone version had a better chance since it would presumably have all the necessary bits of code as part of the install package but to no avail. Is there some underlying install issue with 7.4.0 that has not been resolved yet? Any thoughts?
I had selected MSP430/432, FRAM, and C2000 Compilers along with other options that looked helpful (less other compilers) to include all of the supported emulator/debuggers.
The last failed install log was as follows:
***********start of log
Log started 01/10/2018 at 16:37:16
Preferred installation mode : unattended
Trying to init installer in mode unattended
Mode unattended successfully initialized
[16:37:16] Found mode
Executing C:\Users\kabell\Downloads\ccs_setup_7.4.0.00015.exe --mode win32 &
Script exit code: 0
Script output:
Script stderr:
Cannot delete file C:/Users/kabell/AppData/Local/Temp/bitrock_installer_21388.log
Cannot delete file C:/Users/kabell/AppData/Local/Temp/bitrock_installer_9768.log
[16:37:17] Windows 7 1
[16:37:17] installer_command_line_arguments :
[16:37:17] installer_command_line_arguments :
[16:37:17] Product Name Code Composer Studio 7.4.0
[16:37:17] Product Version 7.4.0.00015
[16:37:17]
Preparing to Install
Preparing to Install
Unpacking files
Unpacking files
Unpacking files
Unpacking files
Unpacking files
Unpacking files
Unpacking files
[16:37:20] admin = 1
[16:37:20] installertype = setup
[16:37:20]
[16:37:20] running C:\Users\kabell\AppData\Local\Temp/ccs_43cc67b5-0a7f-409f-7ba3-75bc90a7fa96\tcl\bin\tclsh "C:/Users/kabell/AppData/Local/Temp/ccs_43cc67b5-0a7f-409f-7ba3-75bc90a7fa96/installer_tcl/main_frontend/main.tcl" --installersrc "C:/Users/kabell/Downloads" --installertmp "C:/Users/kabell/AppData/Local/Temp/ccs_43cc67b5-0a7f-409f-7ba3-75bc90a7fa96" --buildid 7.4.0.00015 --installer "C:/Users/kabell/Downloads/ccs_setup_7.4.0.00015.exe" --bitness 64-bit --os windows --osname "Windows 7" --spversion "1" --timestamp 20180110163717 --AVon false
Executing C:\Users\kabell\AppData\Local\Temp/ccs_43cc67b5-0a7f-409f-7ba3-75bc90a7fa96\tcl\bin\tclsh "C:/Users/kabell/AppData/Local/Temp/ccs_43cc67b5-0a7f-409f-7ba3-75bc90a7fa96/installer_tcl/main_frontend/main.tcl" --installersrc "C:/Users/kabell/Downloads" --installertmp "C:/Users/kabell/AppData/Local/Temp/ccs_43cc67b5-0a7f-409f-7ba3-75bc90a7fa96" --buildid 7.4.0.00015 --installer "C:/Users/kabell/Downloads/ccs_setup_7.4.0.00015.exe" --bitness 64-bit --os windows --osname "Windows 7" --spversion "1" --timestamp 20180110163717 --AVon false
Script exit code: 0
Script output:
Buildfile: c:/ti/ccsv7/eclipse/downloads/ccs_p2_mirror.xml
create-mirror:
BUILD SUCCESSFUL
BUILD SUCCESSFUL
Total time: 6 minutes 35 seconds
Script stderr:
Error from thread tid00002AFC
target thread died
while executing
"thread::send $m_threadId [subst { $m_display reportError {$msg} } ]"
(object "::threadedProgressUpdate0" method "::ThreadedProgressUpdate::reportError" body line 3)
invoked from within
"$progress reportError $msg"
(procedure "RunInstall" line 10)
invoked from within
"RunInstall c:/ti/ccsv7/eclipse/ccs_config.xml 2 0 0 0 c:/ti/ccsv7/install_logs/20180110163717/ccs_setup_7.4.0.00015_install.log ::progressPane0 tid000..."
called Tcl_FindHashEntry on deleted table
[17:22:44] Buildfile: c:/ti/ccsv7/eclipse/downloads/ccs_p2_mirror.xml
create-mirror:
BUILD SUCCESSFUL
BUILD SUCCESSFUL
Total time: 6 minutes 35 seconds
[17:22:44] Error from thread tid00002AFC
target thread died
while executing
"thread::send $m_threadId [subst { $m_display reportError {$msg} } ]"
(object "::threadedProgressUpdate0" method "::ThreadedProgressUpdate::reportError" body line 3)
invoked from within
"$progress reportError $msg"
(procedure "RunInstall" line 10)
invoked from within
"RunInstall c:/ti/ccsv7/eclipse/ccs_config.xml 2 0 0 0 c:/ti/ccsv7/install_logs/20180110163717/ccs_setup_7.4.0.00015_install.log ::progressPane0 tid000..."
called Tcl_FindHashEntry on deleted table
[17:22:44]
launchCCS:0
createDesktopShortcut:0
createStartMenuShortcut:0
eclipsedir:c:/ti/ccsv7/eclipse
***********end of log*********************************
Regards,
Keith Abell
Senior Firmware Enginieer
Intellipower, Inc