This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPA200: VOFFSET/VCC2 filter capacitor

Part Number: DLPA200
Other Parts Discussed in Thread: DLPLCRC410EVM

Hi E2E support,

According to DLPA200 datasheet, a value of VOFFSET/VCC2 filter capacitor is 1-4.7µF.

Note : Recommended value is 3.3 µF each.

      Different values are acceptable, provided that the sum of the two is 6.8 µF maximum.

 

However, 10uF filter capacitors are used for the DLPLCRC410EVM.

Which is correct ?

If the description of the datasheet is correct, why 10uF filter capacitors for the VOFFSET/VCC2 are used in the EVM board?

 

Best Regards,

Koike