This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP for HUD

Other Parts Discussed in Thread: DLP4710

Hi,

We have DLP requriement for HUD which is auto grade 

But the requirement is Full HD resolution , TI has no full hd auto grade IC

so i was looking at pico chisets in which DLP4710 was having temperature range of -20 to 90 which is good and better

but only thing i am not clear is are these pico chipsets suitable for HUD kind of applications

or can use a full HD supported standard chipset and use a heater to achieve lower temperature operation which is -40 degree

kindly suugest best possible solution