Part Number: DLPLIGHTCRAFTER
Hi Team
We have this DLPCR9000EVM evaluation board currently in the group, and I'm testing it to confirm certain characteristics so we could later proceed with the correct model for our application. To get a better knowledge on DMDs, I'd like to inquire some basic info regarding this module (and possibly the DLP9000 chip):
1. So from the 101 document, if I use a global reset, there will be a reset period during which all the micromirrors on the chip will change to its new state. So where can I find this parameter for the DLP9000 chip? I only saw a 'cross-over' time of 2.5us in the spec sheet, but I suppose that's not the actual reset time? Also, during the reset period, does all the mirrors change states simultaneously, or it's actually done in a 'rolling-shutter-fashion' so some micromirrors change first and others later?
2. And when I use the 'pattern on the fly' mode in GUI, it kept reminding me that the dark time should be more than 105us --- so what exactly is this dark time? is it the time to load the CMOS cells plus the reset period? Oh and a related question: the LVDS to this chip is 32-bit like in the 101 document (so updating one row takes 80 clock pulses)?
3. Is it possible to only load and update a subset of the chip in each block? Also I recall Fizix once told me that DLP650LNIR could do this Load4 operation so effectively reducing the load time (I only need to load same patterns across multiple rows in a block), just wondering if it is possible with the DLP9000 chip? And maybe even through the GUI?
4. One last question: I'm curious if it is possible to get larger flash memory on the DLP chip? The DLPCR9000EVM seems to be able to store up to 400 binary patterns, but we might need something up to 1600 patterns.
Thanks,
Yujie Shen