Other Parts Discussed in Thread: DLPA3005, DLPC3439, DLPLCRD-GUI
Hi Lori,
Thanks for your reply.
I can see that the displayed image is 1280x720p as that's what the program is saying (picture below). I also have my own code that checks for resolution and it prints out the same number (2nd picture below).
As you can see in the picture below, the image sent is 1920 x 1080 and then it gets cropped to 1280 x 720 but it's not possible to change this parameter for the 4710 EVM as explained in the asterisk (which is the model that I have).
If the device is sold as full HD it should be displaying full HD not cropping the image, do you know a way this can be changed?
Many thanks,
Valentina