Other Parts Discussed in Thread: DLPC910,
Hello
I'm designing a board with DLP9000X include DLPC910 and DLPR910, which of the components should powered on first the DLP9000X or DLPC910?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Avner,
The component that will be powered on first should be the DLPC910 Controller. Since the DLPR910 PROM provides the clock, this will have to come before the DLPC910 Controller and in order for the DMD and Controller to communicate, make sure the DMD has the appropriate power provided to it.
Avner please ensure you have implemented the SPI flash design update for the DLPC910 as the DLPR910 will soon be EOL.
See DLP® Products Advisory for the DLPR410 and DLPR910 Devices