Other Parts Discussed in Thread: DLP3010, DLPC3478, DLPC3430
I am attempting to flash an image onto the DLP3010, however I am unable to communicate with the board. I am using "DLP EVM GUI" to interface with the board. The board is powered with a 19V power supply. The board is connected to a laptop using USB and the power switch is in the ON position. The board has LEDs that turn on when connected to the power supply. The message for connection at the bottom of the GUI screen states "Connected, powered off". Attached are screenshots of the main screen and screenshots of the errors we received when attempting to connect the board. If there is any further information needed, please let me know.