Other Parts Discussed in Thread: DLPC900
Hi Team,
When I go into system settings and put the LED in manual mode, I get a box of light that comes out of the DMD even though there isn't a pattern selected, the light goes off when I put the LED in automatic mode but then I can't seem to adjust the power. Regardless of the LED mode, I still see that box of light when I start a pattern that I've added in pattern mode. For example, if I add a line, I get a box of dim light all around the pattern so it's not a very clear on/off around the pattern. Do you have a specification for this? Do you have examples of small patterns that you've done with the instrument so I can see what the image looks like? Lastly, are there image creating programs that are non-compatible with this software or is there maybe one you recommend more?
Thank you.
-Mark