Using the GUI, the internal pattern file can be generated as shown below.
However, the maximum pattern number can be generated is only "10" as I tested.
After 10 patterns, it omits extra patterns randomly.
The tested pattern size is 1920x1080, 1-bit vertical pattern.
Thank you.